What is the maximun Lenght of TK850 cable can be used ?
We have requirement to add new CI853 in the existing controller, due to space constraint we need to go with TK850 ( CEX-Bus Extension cable), As per the standard it is only 0.7 meters, Is it possible use the cable more that 0.7 meter or is this customisable ??
Answers
This is described in the AC800M Hardware manual 3BSE036351-600 A
TK850 CEX-Bus Extension Cable Only one TK850 CEX-Bus extension cable may be used in any one CEX-Bus.
Cable length: 0.7 m (2.3 ft).
It's not supported to make a "home made" longer cable"
BR
Jan-Erik
Add new comment