800xA 5.1 RevC FP4 license error annoyance on redundant server and operator clients added without using setup packg
Hello All,
I had an 800xA 5.1 RevC FP4 system as standalone. Without disturbing this existing system, I created three Standalone systems of the same versions and added them as a Redundant server and two Operator clients from the existing system. Now everything is working fine except that i am getting license error annoyance on the newly added system. Valid license(dongle based) for redundant servers with operator clients is loaded on the existing system which works fine for this system.
How do I connect the license to the newly added systems without using setup package ,and get rid of the license error annoyance.
Thanks in advance
I had an 800xA 5.1 RevC FP4 system as standalone. Without disturbing this existing system, I created three Standalone systems of the same versions and added them as a Redundant server and two Operator clients from the existing system. Now everything is working fine except that i am getting license error annoyance on the newly added system. Valid license(dongle based) for redundant servers with operator clients is loaded on the existing system which works fine for this system.
How do I connect the license to the newly added systems without using setup package ,and get rid of the license error annoyance.
Thanks in advance
Answers
Was the old system not redundant at first? Then you will problably need a new license with redundant tags. You need to buy extension to your existing license.
Have a look at the 'License status viewer' > error description, will give a clear information about the license pop-up.
Add new comment