Is it possible to connect S800I/O with S7-400?
Dear colleagues,
I would like to know if there is any communication interface (CI) that connects S800I/O with a Siemens PLC S7-400? Or is there another way to make this communication happen?
Thanks in advance
I would like to know if there is any communication interface (CI) that connects S800I/O with a Siemens PLC S7-400? Or is there another way to make this communication happen?
Thanks in advance
Voted best answer
Hi,
This should be with using of CI801 or CI830 (with GSD file/s) for S800IO and connect them as slave to S7-400.
Look in the following posts:
http://www402.abbext.com/Adding-ABB-I...
https://support.industry.siemens.com/tf/ww/en/posts/21713/
This should be with using of CI801 or CI830 (with GSD file/s) for S800IO and connect them as slave to S7-400.
Look in the following posts:
http://www402.abbext.com/Adding-ABB-I...
https://support.industry.siemens.com/tf/ww/en/posts/21713/
Add new comment