Freelance Upgrade - Version 8.1.4271 - to Freelance 2016 SP1
Hi All
Could someone guide me route to upgrade.
Currently running Version 8.1.4171 onsite, Do I update the controller with intermediate version OR can I upgrade the firmware straight to Version 2016 SP1.
Regards
Could someone guide me route to upgrade.
Currently running Version 8.1.4171 onsite, Do I update the controller with intermediate version OR can I upgrade the firmware straight to Version 2016 SP1.
Regards
Voted best answer
You can upgrade the firmware in one step.
But you have to upgrade the cbf project (usersoftware) across all intermediate versions.
That means generate a csv file in V8.1, import in V9.x,check. Export a csv in V9.x import in V13...
export V13, import V16SP1.
Note regarding the version:
V2016 SP1 is not the last stand.
It would be better to use the Roll Up RU03 (Several fixed problems included)
Please note!!
Before you generate the csv file in V8.1 you have to do a parameter upload from all parameters, which are necessary for the process
(KP, TN, Delay times, limits)
But you have to upgrade the cbf project (usersoftware) across all intermediate versions.
That means generate a csv file in V8.1, import in V9.x,check. Export a csv in V9.x import in V13...
export V13, import V16SP1.
Note regarding the version:
V2016 SP1 is not the last stand.
It would be better to use the Roll Up RU03 (Several fixed problems included)
Please note!!
Before you generate the csv file in V8.1 you have to do a parameter upload from all parameters, which are necessary for the process
(KP, TN, Delay times, limits)
Answers
I had this pop on my Logs....
Any suggestions what I can check for. Check all my network Comms.
Any suggestions what I can check for. Check all my network Comms.
by Yagishen Rank: 287 on 1/7/2019 11:10:29 PM | Like (0) | Report
Hi All
After I have upgraded from 8.14 to 2016 SP1 RU3 - Noticed intermittent Communication to Internet Card - Goes to Orange state. Reset controller fixes issue.
Anyone seen this before.
Add new comment