Connecting soft controller for 800xA
Hi,
I am trying to connect soft controller for 800xA V5.1 but not getting success in doing that. I am using a virtual machine Windows Server 2008 R2 standard and trying to connect through local host with ip address 127.0.0.1:2. Please also see the image file for 800xa version install on this VM. soft controller was not initially install with 800xa, later I installed it by copying setup file of soft controller from some other machine. Please help me to resolve this issue.
Thanks & Best Regards,

I am trying to connect soft controller for 800xA V5.1 but not getting success in doing that. I am using a virtual machine Windows Server 2008 R2 standard and trying to connect through local host with ip address 127.0.0.1:2. Please also see the image file for 800xa version install on this VM. soft controller was not initially install with 800xa, later I installed it by copying setup file of soft controller from some other machine. Please help me to resolve this issue.
Thanks & Best Regards,

Answers
1. Install the Softcontroller on the AC800M Connectivity Server.
2. Start the Softcontroller.
3. Configure the OPC Server for AC 800M (The smily face tool) with the IP address of the Connectivity Server with a added :2 (eg. 172.16.4.21:2) for both DA and AE
4. In CB change the controller IP to match the Softcontroller IP ie. 172.16.4.21:2 (again with the :2) added.
5. Download
2. Start the Softcontroller.
3. Configure the OPC Server for AC 800M (The smily face tool) with the IP address of the Connectivity Server with a added :2 (eg. 172.16.4.21:2) for both DA and AE
4. In CB change the controller IP to match the Softcontroller IP ie. 172.16.4.21:2 (again with the :2) added.
5. Download
Add new comment