Problem in cp651 to update runtime
I have cp651 and panel builder and 1.90 . I have set ip address of cp651 as 192.168.1.10 and my laptop ip as 192.168.1.9 whr Panel builder1.90 . System is pinging with cp651 . But when i m going to update runtime or download project its shows error target is not detected as attached in pic
Answers
Hi,
I can't see your picture attached. Beside the setting of IP addresses for the panel and the PC, you need to select the IP of your panel prior to downloading the project.
Do you see the panel's IP when select Download...? With the settings below it is working with me:

I can't see your picture attached. Beside the setting of IP addresses for the panel and the PC, you need to select the IP of your panel prior to downloading the project.
Do you see the panel's IP when select Download...? With the settings below it is working with me:
Add new comment