What is the latest version of McAfee supported by 800xA 5.1?
Hello
In the document 3BSE041902 - System 800xA - Third Party Security Updates Validation Status it is written that
"The latest testing was done with the following versions of 3rd party software installed:
Version: 8.8.0 (8.8.0.1982)
Scan Engine: 5900.7806 "
Also there is an information in this document that Patch 11 is also supported:
"Qualified McAfee Virus Scan® Enterprise 8.8 with Patch 11"
I have registered on McAfee Business Support portal and the latest Patch available there is Patch 8.
Where I can find information about Patch 9, 10 and 11? And what is the latest officially supported Patch by 800xA 5.1?
Answers
Hi,
the document 3BSE041902 - System 800xA - Third Party Security Updates Validation Status document applies to System 800xA version 5.1. So patch 11 is qualified.
BR
ATP
Add new comment