P&P object displays not showing all values in Smart Client
In our 800xA version 5.1 we are using the PID controller PID01A from the pulp and paper library 5.3-2. In smart client 2.3-0 the object display is only showing a very limited number of values. See the screen caption. Similar can be seen in some other pulp and paper object displays, e.g. DriconS (unit for variable speed motor).
Do anyone know if there is a solution to this? Is this a problem related to our versions and fixed in newer versions?
Thanks, Tor
Voted best answer
There is a timeout issue in SC 2.2 Rev C RU2B that will be resolved in the coming RU3 (was initially supposed to be released in September).
The first time you open an object display you only get to see some data, if you reopen the same display all items will be shown.
I was working with the support persons during march and we confirmed it to be a timing issue (timeout to short).
The first time you open an object display you only get to see some data, if you reopen the same display all items will be shown.
I was working with the support persons during march and we confirmed it to be a timing issue (timeout to short).
Answers
Hi!
Not an expert of P&P, but could attributes be "hidden" (from OPC)?
Regards
Not an expert of P&P, but could attributes be "hidden" (from OPC)?
Regards
The first question would be, is this display of "Category Name", "Graphic Display PG2" in the Aspect view. These are they only types that are able to be imported into Smart Client. Second would be, does this Display have any "Aspect Wrapper" or "ActiveX" elements, as these are not capable of being displayed as yet in Smart Client.
The most recent released version of Smart Client is ver. 2.2 RevC RU2b. If you are truly running SC 2.3-0, I would assume that this is the Beta Version that was released in late 2015 or early 2016 to obtain enhanced Cyber Security capability. If so, this version of Smart Client was originally based on an early version of Smart Client 2.2 RevC, (I believe). As such, it was not capable of receiving any of the latest corrections that happened after the initial Beta release. The newest version of Smart Client 2.3 is due out very soon, (originally Nov 2018), and will contain most all of the current upgrades. There is also an upgrade due out for SC 2.2 RevC RU2b, to 2.2 RevC RU2c, due out at the end of January 2019, is the latest I have heard.
Regards,
Geof Ledin
The most recent released version of Smart Client is ver. 2.2 RevC RU2b. If you are truly running SC 2.3-0, I would assume that this is the Beta Version that was released in late 2015 or early 2016 to obtain enhanced Cyber Security capability. If so, this version of Smart Client was originally based on an early version of Smart Client 2.2 RevC, (I believe). As such, it was not capable of receiving any of the latest corrections that happened after the initial Beta release. The newest version of Smart Client 2.3 is due out very soon, (originally Nov 2018), and will contain most all of the current upgrades. There is also an upgrade due out for SC 2.2 RevC RU2b, to 2.2 RevC RU2c, due out at the end of January 2019, is the latest I have heard.
Regards,
Geof Ledin
Add new comment