800xA Logged User
Hello everybody
I wonder if in the 800xA system is included a boolean property
that reveals if a particular user is logged onto the system, basically
to make it possible enabling or disabling a PG2 graphic object
dinamically, based on the logged/authenticated user.
thanks a lot
P.Besazza
Answers
A similar requirement has been answered in the thread: https://forum-controlsystems.abb.com/...
Yes. But ... That's not how 800xA Security works.
Security is based on Rights and Roles. If you don't have the correct role, then you cannot operate the object. Rights and roles are controlled by the System Configuration Console in version 6 and by the System Configuration Wizard in earlier versions.
Read the manuals on System Configuration and Security for details. Trying to work around the security model by accessing the ID of the logged in users can lead to serious problems later if the customer wants to add or remove users.
Security is based on Rights and Roles. If you don't have the correct role, then you cannot operate the object. Rights and roles are controlled by the System Configuration Console in version 6 and by the System Configuration Wizard in earlier versions.
Read the manuals on System Configuration and Security for details. Trying to work around the security model by accessing the ID of the logged in users can lead to serious problems later if the customer wants to add or remove users.
Add new comment