Sir I have ACS 880, 59 Amp, 415 v drive...it was kept in store since 2016..I want to use it now.. capacitor reform
Capacitor reformation is required for it or not? If yes then how?
Voted best answer
Hi
capacitor reforming is one good practice of maintenance for every type of drives.
You can find one guide for the reforming operation at the follow link:
http://search-ext.abb.com/library/Dow...
Hope this help you
capacitor reforming is one good practice of maintenance for every type of drives.
You can find one guide for the reforming operation at the follow link:
http://search-ext.abb.com/library/Dow...
Hope this help you
Answers
Hi,
If the drive module has been stored for a year or more, reform the capacitors. Electrolytic DC capacitors in the converter module DC link need to be reformed (re-aged) if the module has been non-operational for a certain time. Without reforming, the capacitors can get damaged when the converter starts to operate.
Refer capacitor reforming instructions (3BFE64059629 [English])
BR
ATP
If the drive module has been stored for a year or more, reform the capacitors. Electrolytic DC capacitors in the converter module DC link need to be reformed (re-aged) if the module has been non-operational for a certain time. Without reforming, the capacitors can get damaged when the converter starts to operate.
Refer capacitor reforming instructions (3BFE64059629 [English])
BR
ATP
Add new comment