Arduino signals integrated to DCS system...
I'm interested to use a Arduino microcontroller that reads a signal from I2C device and activates a relay output, then send that signal to DCS using DI810 module. In guess there is not any problem doing that.
If you have any opinion about what others things do I need to consider in order to integrate Arduino with DCS I will appreciate that.
If you have any opinion about what others things do I need to consider in order to integrate Arduino with DCS I will appreciate that.
Voted best answer
Greetings,
For integration you have two options:
Or you can find any other protocols, which is suitable for you hardware.
Hope it helps you.
For integration you have two options:
- Hardwire (as you do with DI810 Module)
- Communication Protocol.
Or you can find any other protocols, which is suitable for you hardware.
Hope it helps you.
Add new comment