Differentiate audible alarms by user
Hello, we have a 800xA 6.0.3 using tabbed workplace mode. The customer want to differentiate the sound or enable or disable the sound depending the logged user. Is possible to do this using the same workplace?
Regards.
Regards.
Voted best answer
As sounds are based on the workplace being opened, you would have to create a different workplace with different sounds. As you could copy the WP anyway, this should not be too much of a problem, just keep the "first" one as your master, as you need to make changes to, just keep copies of the aspect with the sound changes.
Answers
No.
A trick (not tested) could be to have a login script to juggle the .wav or .mp3 files that the Audible Alarm Configuration is pointing to...
A trick (not tested) could be to have a login script to juggle the .wav or .mp3 files that the Audible Alarm Configuration is pointing to...
Add new comment