800xA DataDirect in V6.0.3.2
800xA Version 6.0.3.2
ES OS Version - Windows 10 Ent 2016 LTSB
MS office - MS office Standard 2016
Will DataDirect work in this MSOffice standard 2016, if only Pro Plus is allowed then is there any alterante method to make Office standard to work effectively for all 800xA Data Direct components.
ES OS Version - Windows 10 Ent 2016 LTSB
MS office - MS office Standard 2016
Will DataDirect work in this MSOffice standard 2016, if only Pro Plus is allowed then is there any alterante method to make Office standard to work effectively for all 800xA Data Direct components.
Voted best answer
Hello Mok,
As per the System 800xA - 3rd party software versions manual, from SV 6.0.2 onwards, along with MS Office 2016 standard, even Office 2016 Pro Plus is supported. So, it should not be any problem if you use any.
Only doubt I have is if have installed 64-bit version of Excel. Supported version is 32-bit.
As per the System 800xA - 3rd party software versions manual, from SV 6.0.2 onwards, along with MS Office 2016 standard, even Office 2016 Pro Plus is supported. So, it should not be any problem if you use any.
Only doubt I have is if have installed 64-bit version of Excel. Supported version is 32-bit.
Answers
It is the Excel version that is important not the Office bundling (eg Office Standard Vs ProPlus). As 800xA 6.0.3.2 support Office 2013-2016 (from memory) then this should pose a problem.
by Mok_6430 Rank: 156 on 11/13/2018 9:09:34 AM | Like (0) | Report
I am facing error when try to add or use Datadirect add in
And error says "Compile error in hidden module: AECollClass
This error is same when tried with Both MSOffice Standard and Pro Plus
Add new comment