How to download again a program in HMI CP650 WEB restored from factory, i can´t acces to main ios
Answer this question FollowVoted best answer
1. In “System settings” set the IP address of the panel
2. Connect from the PC with PanelBuilder to the panel by means of ethernet port
3. Start PanelBuilder: Run -> Download to Target.
The First time may be you will need to load the runtime (Update Runtime), just follow the instruction in the software
Add new comment