Wrong file format when import of PRT-file
Hello,
when I try to import a program part from one Freelance project to another project I get the error Wrong file format.
Both projects are 2016 SP1 but the .PRT file was created in a W10 PC and imported to a W7 PC.
I have checked the .PRT file and it is UNICODE.
Very best
/tore
when I try to import a program part from one Freelance project to another project I get the error Wrong file format.
Both projects are 2016 SP1 but the .PRT file was created in a W10 PC and imported to a W7 PC.
I have checked the .PRT file and it is UNICODE.
Very best
/tore
Answers
Hello Tore,
we checked:
Can you post the PRT file that makes trouble?
we checked:
- Export one FBD with Freelance 2016 SP1 / Win 10 (64-bit)
- Import the PRT-file withFreelance 2016 SP1 / Win 7 (32-bit)
Can you post the PRT file that makes trouble?
Hello Dieter,
Attached prt file.
Attached prt file.
Source: From New thread - /Admin
I imported the PRT file just fine. No error. I have a Freelance 2016SP1 [10.3.9142] installation on Win 7 64 Bit. I choose menu Edit / Import Block while in the P-Tree.

Do you import into a Win7 32 Bit or into a Win7 64 Bit?
Do you import into a Win7 32 Bit or into a Win7 64 Bit?
Add new comment