CP661 Splash Page with user login
I am using a CP661 Touch Screen on a control project. I have implemented some security so each user has to log in before being able to do anything within the system. I would like like to implement an alarm screen where anyone walking by can see if there are any alarms. I don't want to allow any changes, acknowledge the alarm, or any type of user interaction without logging in. I just want them to be able to view this page. I currently have the alarm page, however they have to login before they can see this screen. Does anyone know if this is possible to do.
Thanks,
Thanks,
Answers
Do you want to modify your current alarm list security settings or do you want to get rid of the buttons related to that alarm list? UserGroups have "Authorization Settings" where you can modify the security settings of individual page elements. Also default user is automatically logged in when there is system start up or any type of log out. Make sure that this default user isn't under category "Unauthorized". If you want to remove the buttons from alarm list then select the alarm list, right click and select "Convert To Group". Then select "Ungroup". Now you can delete unnecessary objects.
Add new comment