PM573-ETH GSD
Hello, ABB.
Does anyone know where to find or have the GSD file for the PM573-ETH PLC? I can't find anywhere online, including the ABB portal.
Thanks a lot!
Does anyone know where to find or have the GSD file for the PM573-ETH PLC? I can't find anywhere online, including the ABB portal.
Thanks a lot!
Voted best answer
You can download the gsd file here:
http://search-ext.abb.com/library/Dow...
There is gsd file named ABB_091F.gsd, where is module PDP22-FBP (DPV1 modular) with several parameters named like "PM5X1 xx bytes/words in/out". These should match your Automation builder HW configuration.
http://search-ext.abb.com/library/Dow...
There is gsd file named ABB_091F.gsd, where is module PDP22-FBP (DPV1 modular) with several parameters named like "PM5X1 xx bytes/words in/out". These should match your Automation builder HW configuration.
Answers
Greetings,
CM572 Profibus-DP module (for the ABB AC500 PLC family) can act as a Profbus-DP master.
However, GSD files are only used for master-slave communications over Profibus-DP. The GSD file contains information that the Profibus configurator will use to set the parameters of the master's bus profile and data exchange with the slaves. It serves no purpose for master-master communications. So basically you will never find a GSD file for a Profibus-DP master.
Maybe best way for your application is use DP/DP Coupler.
Hope it helps you.
If you need the PM573-ETH to be slave on Profibus you have to use the communication module CM582-DP.
You can find the GDS for CM582 her: http://search-ext.abb.com/library/Dow...
by Steen Rank: 310 on 11/2/2018 3:04:44 AM | Like (0) | Report
If you need the PM573-ETH to be slave on Profibus you have to use the communication module CM582-DP.
You can find the GDS for CM582 her: http://search-ext.abb.com/library/Download.aspx?DocumentID=1SAP192501R0160&LanguageCode=de&DocumentPartId=&Action=Launch
Add new comment