ACS800 - AINT-02C fault
Dear Experts
I use ACS800-04M-0260-3 for hoisting. I have a trouble, please help me why
Before The fault is PPCC link 5210 - and DC BUS V is 0.0, actual 545 VDC, ACS 800 temp -7,1% AC Voltage 415V, actual 390V look on panel - then I replace AINT-02C board
may-2017 I replace new ACS800 - now October-2018 I get the same fault.
I attach the photo of led - led 5V no light
I do not know why - the same position - the same fault.
Thank you very much!
I use ACS800-04M-0260-3 for hoisting. I have a trouble, please help me why
Before The fault is PPCC link 5210 - and DC BUS V is 0.0, actual 545 VDC, ACS 800 temp -7,1% AC Voltage 415V, actual 390V look on panel - then I replace AINT-02C board
may-2017 I replace new ACS800 - now October-2018 I get the same fault.
I attach the photo of led - led 5V no light
I do not know why - the same position - the same fault.
Thank you very much!
Answers
Hi
a diagnosis that can give you an answer is only possible by analyzing the components and all the boundary conditions.
In these cases, I can only suggest that you contact ABB's Service, which is made up of the best specialists in the sector. They can also support you in the best possible choice of possible actions to be implemented
Hope this help you
a diagnosis that can give you an answer is only possible by analyzing the components and all the boundary conditions.
In these cases, I can only suggest that you contact ABB's Service, which is made up of the best specialists in the sector. They can also support you in the best possible choice of possible actions to be implemented
Hope this help you
Add new comment