problems when deleting a library
hello, I'm having problems when trying to delete a library of an application, since it tells me that it is in use, by doing a bulk to check the types of blocks that are being used in the application, it throws me that no block of the library to erase (Infi90SUPPlib 2.0) is being used, even though it does not allow me to erase it and it warns me that there are types in use
Answers
Greetings,
Maybe you just connected the library and did not use in the application. It causes the same error message.
You can Right Click the related library and choose "Library Usage" option.
It indicates, where did you use the library or connect the library.
Hope it helps you.
Maybe you just connected the library and did not use in the application. It causes the same error message.
You can Right Click the related library and choose "Library Usage" option.
It indicates, where did you use the library or connect the library.
Hope it helps you.
In addition to the other advise - look if this library is not connected to the other library in the project
Add new comment