Getting temparary license error popup after connecting Operating stations/engineering stations through remote desko
Getting temparary license error popup after connecting Operating stations/engineering stations through remote desktop from other PC(non 800xA and other 800xA systems) 800xA version 5.0 SP2.
any solution.?
any solution.?
Answers
Until recently, two operator licenses were in use:
These licenses are not interchangeable. Users entering via RDP need a REM_OPER_WPL license seat, or else license annoyance will be present.
- OPERATOR_WPL
Allocated by workplace when launched on console - REM_OPER_WPL
Allocated by workplace when launched via Remote Desktop Protocol (RDP)
These licenses are not interchangeable. Users entering via RDP need a REM_OPER_WPL license seat, or else license annoyance will be present.
Hi,
As explained by stefan, you can verify the license usage and feature in Admin Structure-->Administrative structure-->domain -->License usage.
Verify the features. If Remote WPL is not there, request for the additional feature.
As explained by stefan, you can verify the license usage and feature in Admin Structure-->Administrative structure-->domain -->License usage.
Verify the features. If Remote WPL is not there, request for the additional feature.
Add new comment