How import .icd file from Alstom p14d to Ref615
i exported .icd file from p14d and then imported to ref615, I can see ınputs in pcm600-(Goose Configuration-inputs) , I made gooserscv function block in pcm and finally i opened signal matrix but I couldn’t select don’t allow
please help me
please help me
Answers
I think you are supposed to import the p14d icd to a generic IEC 61850 IED in PCM600, not to REF615. Have you looked at "615 series IEC 61850 Engineering Guide"? ( https://search.abb.com/library/Downlo...). There Section 5 have quite good instructions how to create the GOOSE configuration.
If you think that you have configured the IEDs correctly, but PCM600 just don't allow you to make the connections in Signal Matrix and the background of the cells is red, then it means that the IEC 61850 datatypes don't match. For example PCM600 don't allow connecting analog signal to binary signal.
If you think that you have configured the IEDs correctly, but PCM600 just don't allow you to make the connections in Signal Matrix and the background of the cells is red, then it means that the IEC 61850 datatypes don't match. For example PCM600 don't allow connecting analog signal to binary signal.
Add new comment