ABBLicenseservice cannot be found
In my aspect server, I fount the ABBLicenseService warning as per attached picture. What is the meaning of this warning. My client license service provider is running normally.Could anybody help?
Voted best answer
Hello,
These messages are being generated by the licensing node, but really caused by IIS application pools. This is a behavior of IIS restarting. 30 hours is the default application pool reset time. Microsoft does this periodically to cleanup resources and is a normal behavior. This will only be a problem it the systems do not recover in a timely manner. Sufficient reconnection logic is provided in the license client to prevent any notices being popped up to the user. The message being displayed only indicates that the new connection has been made to the aspect server (system).
If required, you can contact your regional support center for more information.
by ATP
Attachment missing..
by Teleng Rank: 236 on 10/29/2018 12:20:35 AM | Like (0) | Report
Refer attached picture
Add new comment