Auto pin facplates in CHMI
Dear All,
Is there any way to pin 📍 the faceplates automatically in compact HMI.
Now, every time i open a faceplate all other unpinned faceplates close.
Regards,
Abdelrazzaq Hiasat
Is there any way to pin 📍 the faceplates automatically in compact HMI.
Now, every time i open a faceplate all other unpinned faceplates close.
Regards,
Abdelrazzaq Hiasat
Voted best answer
Answers
When there is a faceplate on the screen and another is selected, the normal behavior is to replace the first faceplate. There is however possible to configure the Operator Workplace to be able to show several faceplates at the same time. This may be done resulting in two different behaviors. All faceplates that are brought up are displayed separately. Each faceplate needs to be removed separately. The maximum number of simultaneous faceplates is configurable and the default number is five.
The replacement strategy shall be Preserve instead of Replace.
The replacement strategy shall be Preserve instead of Replace.
Please see this link about setting the pin button to on in every faceplate, also , under the same path you will see the offset parameter that also helps to custimize when several faceplates are open
https://forum-controlsystems.abb.com/...
https://forum-controlsystems.abb.com/...
Add new comment