Does Touch PanelPP877 supports alarm event translation when when collecting alarms ,events directly from AC800 ?
Does Touch Panel 10.4" PP877 HMI (panel builder v6.0)supports alarm event translation when collecting alarms and events generated directly from AC800 via AE subsciption on AC800 for example using Alarmcond and Simple event detector function block and not via MMS variables.?
Does Panel have some kind of alarm and event translator aspect functionality like 800xA?
Does Panel have some kind of alarm and event translator aspect functionality like 800xA?
Answers
I believe not.
I think you just have to configure the text in the panel if you are subscribing events from AC800
But it has got multiple system language support
Panel Builder supports multilingual applications. Translation of texts and system texts can be performed directly in the application, or via export to a text file to be translated in other software.
The file is imported to the application after translation. The application language can be changed in runtime, for example based on a tag value.
Add new comment