Uplaod&Download to AC800M
Hi,
Lets say this is our first time to get connected to a CPU of AC800M series and we do know the IP adresse of that CPU.
Is there any possibility to Uplaod the project from AC800M (PM866) to CBM like SIEMENS option -PLC TO PG- ?
How can we save the hole project also like SIEMENS option -ARCHIVING THE PROJECT- without going trough the Engineering tools export import?
thanks in advance.
Lets say this is our first time to get connected to a CPU of AC800M series and we do know the IP adresse of that CPU.
Is there any possibility to Uplaod the project from AC800M (PM866) to CBM like SIEMENS option -PLC TO PG- ?
How can we save the hole project also like SIEMENS option -ARCHIVING THE PROJECT- without going trough the Engineering tools export import?
thanks in advance.
Answers
Hi,
You have to set the IP of the AC800M as per your design . Use the IP config tool to set the IP and the procedure is available in the help file itself. The IP setting cable will be available with the controller package.
There is no option to upload the project from the AC800M. You can take compact backup of the control builder.
You can take the 800XA maintenance backup it will includes all the backup.
You have to set the IP of the AC800M as per your design . Use the IP config tool to set the IP and the procedure is available in the help file itself. The IP setting cable will be available with the controller package.
There is no option to upload the project from the AC800M. You can take compact backup of the control builder.
You can take the 800XA maintenance backup it will includes all the backup.
To put it simple:
No, the ABB AC 800M only permit download of an application.
No, the ABB AC 800M only permit download of an application.
Add new comment