Connecting aztec600(profibus slave) to gateway(profibus-modbus) to rvg200(modbus master)
Hello everyone,
I hope you can help me solve this issue. I have aztec600 with 4 variable inputs and act as profibus slave with byte 1 to 4 = input 1; byte 5 = status AI1; byte 6 to 9 = input 2 and so on then gateway converts profibus byte 1 to 4 into byte 0 to 3 in modbus protocol and RVG200 as a master and i can call AI byte 0 to 3: I just input address: 1, register 0 and data type IEEE.
My problem is the AI 2 and AI4, how can i call them in RVG200??

Best Regards,
I hope you can help me solve this issue. I have aztec600 with 4 variable inputs and act as profibus slave with byte 1 to 4 = input 1; byte 5 = status AI1; byte 6 to 9 = input 2 and so on then gateway converts profibus byte 1 to 4 into byte 0 to 3 in modbus protocol and RVG200 as a master and i can call AI byte 0 to 3: I just input address: 1, register 0 and data type IEEE.
My problem is the AI 2 and AI4, how can i call them in RVG200??

Best Regards,
Answers
This question has not yet been answered.
by algarellano Rank: 2886 on 10/16/2018 5:55:57 AM | Like (0) | Report
Hello,
Can anyone answer this??
Thank you..
by Emil Lopez Rank: 2362 on 11/8/2018 2:24:12 AM | Like (0) | Report
Hi,
Apologies for the late response. I am working on this and I will get back to you as soon as I have an answer.
In the mean time if you have any question feel free to contact me at emil.lopez@gb.abb.com
Regards
Emil
Add new comment