Load cell module
hey
my application is to make batching system , and i need a load cell module to connected with ac500 eco , so what to do in this case since there is no special module for load cell in ABB AC500 ECO .
Another thing is there any example for automatic batching system with 3 gate using codesys , i mean the operator set the needed weight and push a start button the system will open gate one until reaching the desired weight then close gate number one and open gate number 2 ..?
last thing dose abb have scada system if ineed to control and monitiring a big factory ?
thank you .
my application is to make batching system , and i need a load cell module to connected with ac500 eco , so what to do in this case since there is no special module for load cell in ABB AC500 ECO .
Another thing is there any example for automatic batching system with 3 gate using codesys , i mean the operator set the needed weight and push a start button the system will open gate one until reaching the desired weight then close gate number one and open gate number 2 ..?
last thing dose abb have scada system if ineed to control and monitiring a big factory ?
thank you .
Answers
Hi
to use load cell with input in AC500 eCo cpu, you need apposite amplifier for load cell that have analog output o other linearized signal corresponding to min-max load. The output linearized signal from the amplifier can be used by the cpu for every type of regulation.
Examples for batching system could be find with one accurate search on the web.
ABB have more types of DCS for control and monitoring big factory, for example AC800 series. For more information you can contact your local ABB dealer network
Hope this help you
to use load cell with input in AC500 eCo cpu, you need apposite amplifier for load cell that have analog output o other linearized signal corresponding to min-max load. The output linearized signal from the amplifier can be used by the cpu for every type of regulation.
Examples for batching system could be find with one accurate search on the web.
ABB have more types of DCS for control and monitoring big factory, for example AC800 series. For more information you can contact your local ABB dealer network
Hope this help you
Add new comment