Freelance communication to AC800M HI in a SIL3 application?
Hi All,
Can Digivis communicate to an AC800M HI SIL3 Controller via opc with read/write in a SIL3 application?
Can Digivis communicate to an AC800M HI SIL3 Controller via opc with read/write in a SIL3 application?
Answers
Hello Lance,
not that I know. Not with AC 800M HI.
There are Solutions available for Siemens, Hima and AC500 with DigiVis created by a channel partner. You can talk to Peter Rother for Details.
not that I know. Not with AC 800M HI.
There are Solutions available for Siemens, Hima and AC500 with DigiVis created by a channel partner. You can talk to Peter Rother for Details.
OPC or Modbus communication cannot be used for the SIL 3 data transfer. Best way to connect via hard wired signals
Greetings,
If you want to use Digivis just for monitoring signals, you can use OPC Server to get datas from HI CPU.
But you can not use these datas in Freelance CPU etc. it is not possible.
Hope it helps you.
If you want to use Digivis just for monitoring signals, you can use OPC Server to get datas from HI CPU.
But you can not use these datas in Freelance CPU etc. it is not possible.
Hope it helps you.
Add new comment