Bilingual Language, multi languuage support for Touch Panel 10.4" PP877
Our customer need to display HMI panel interface, screen and alarms and events with bilingual language (English and Bulgarian) on the same time, and they can switch between two options whenever they want. Can we do this? And how to do?
Voted best answer
Hi,
I think yes, that is possible. We did that with previous version of panel builder 5.1 and it works.
Looking in the actual version,it is described as possible, even seems to be improved:
"Panel Builder supports multilingual applications. Translation of texts and system texts can be performed directly in the application, or via export to a text fi le to be translated in other software. The fi le is imported to the application after translation.
The application language can be changed in runtime, for example based on a tag value.
The multiple languages con fi guration pages consist of the Texts, System Texts and Languages tabs."
I think yes, that is possible. We did that with previous version of panel builder 5.1 and it works.
Looking in the actual version,it is described as possible, even seems to be improved:
"Panel Builder supports multilingual applications. Translation of texts and system texts can be performed directly in the application, or via export to a text fi le to be translated in other software. The fi le is imported to the application after translation.
The application language can be changed in runtime, for example based on a tag value.
The multiple languages con fi guration pages consist of the Texts, System Texts and Languages tabs."
Source: 3BSE069489-601
Add new comment