Is it possible to integrate some kind of animation or movie (avi,mpg, Xlo) in process graphics? PG2
Is it possible to integrate some kind of animation or movie (avi,mpg, Xlo) in process graphics? PG2 for example displaying windmill rotating ?
thanks in advance
thanks in advance
Answers
If you can live with "some kind of animation" then yes, you can create animations like rotating stuff directly in PG2.
Execute the batch file LoadNewGraphicsDemo.bat located in the folder C:\Program Files (x86)\ABB 800xA\Base\demo, then check Functional Structure / New Graphics Demo / Animations for some example.
Execute the batch file LoadNewGraphicsDemo.bat located in the folder C:\Program Files (x86)\ABB 800xA\Base\demo, then check Functional Structure / New Graphics Demo / Animations for some example.
Hello,
It is not possible to add .avi or .mpg in PG2 graphics. You will have to create animation of your own.
It is not possible to add .avi or .mpg in PG2 graphics. You will have to create animation of your own.
Add new comment