Use the PLC Multiprog software for the SCO, DCO command is configured by RTU560
Hi experts!
I work regularly with ABB RTU560. Currently I am doing software interlock for control commands. However, I have no idea what to do
For example: In RTUtil560 version 12.2.0 I configured 1 binary in put card, 1 binary output card. Input card get LOCAL / REMOTE switch status, Output card for output control such as Circuit breaker.
I want to use the application PLC Multiprog to lock the control from the Control Center when the switch is at the LOCAL, the Control Center only control when switch is at the REMOTE.
With the above requirements, how to program in PLC Multiprog Software. I'm programming in "Function Block" format.
I look forward to receiving answers from experts
Thanks and best regards
Minh Hoang.
I work regularly with ABB RTU560. Currently I am doing software interlock for control commands. However, I have no idea what to do
For example: In RTUtil560 version 12.2.0 I configured 1 binary in put card, 1 binary output card. Input card get LOCAL / REMOTE switch status, Output card for output control such as Circuit breaker.
I want to use the application PLC Multiprog to lock the control from the Control Center when the switch is at the LOCAL, the Control Center only control when switch is at the REMOTE.
With the above requirements, how to program in PLC Multiprog Software. I'm programming in "Function Block" format.
I look forward to receiving answers from experts
Thanks and best regards
Minh Hoang.
Answers
This question has not yet been answered.
Add new comment