Manual for configuration of the interlock display/ Faceplate link creator?
Hello,
i tried to add the interlock display for an user defined function block but I failed. I searched for a manual for the configuration of the interlock display but did not find something fitting.
The system is 800xA 5.1 FP4
Thanks
i tried to add the interlock display for an user defined function block but I failed. I searched for a manual for the configuration of the interlock display but did not find something fitting.
The system is 800xA 5.1 FP4
Thanks
Answers
You said you're using PCDeviceLib, so I assume you want to create the PCC interlock display? Did you add your user defined control module to the PCC Devices aspect in the Library Structure -> Preferences & Customizations -> PCDeviceLib Customizations?
by Rob Lyon
What Libraries are you using for your project ? ( Eg Pulp & Paper, BMI, PC Device Lib etc)
by Matzats Rank: 590 on 10/1/2018 3:39:40 AM | Like (0) | Report
PC Device Lib
Add new comment