Any limitation of using L3 Switch in ABB Control system Network
is there any limitation of using L3 switch in ABB Control system network.
800XA 6.0.3.2
Control Network this will use the L2 switch
Plant Network this will use the L2 switch
L3 switch at main receiving station was suggested by Switch vendor due to RSTP limitation. As number of switch are more than 60.
800XA 6.0.3.2
Control Network this will use the L2 switch
Plant Network this will use the L2 switch
L3 switch at main receiving station was suggested by Switch vendor due to RSTP limitation. As number of switch are more than 60.
- Management switch ( Switch management , Server backup) L3 Switch
- DNP3 Network ( L3 switch - Only the main switch which connects are areas)
Answers
There are several articles on the web explaining the differences between a L2 and a L3 switch.
A L3 switch may also act as a router.
Normally, a router does not forward any multicast traffic between the different IP subnets it connects.
RNRP relies on that the multicasted telegrams it emit reaches all nodes of an RNRP Area (=IP subnet).
Depending on what you had in mind with the L3 switch, it may or may not work for System 800xA.
RNRP can act as a router between different RNRP Areas in:
A L3 switch may also act as a router.
Normally, a router does not forward any multicast traffic between the different IP subnets it connects.
RNRP relies on that the multicasted telegrams it emit reaches all nodes of an RNRP Area (=IP subnet).
Depending on what you had in mind with the L3 switch, it may or may not work for System 800xA.
RNRP can act as a router between different RNRP Areas in:
- a computer with at least two network cards and running the ABB RNRP Windows Service
- ABB NE87x RNRP Router. The NE870 has 11 network interfaces while the smaller NE871 offers 3.
Add new comment