Is it possible to Configure Line Faults from Namur sensors with the PROFIBUS GSD file importadvanced configuration
Hello,
our customer is going to use some IO-cards from Pepperl Fuchs for Namur porposes. These io-cards have a line fault detection for every input, see bit structure below.

One way to use this Line Fault is to create a second BoolIO for every input and give an error on the Line Fault when this occurs. But I also found another option when I click 'Advanced Configuration' in the Custimize input area. See printscreen below:

If I use this, I don't have to program a second boolIO for the Line Fault. But I never used the Advanced Settings before. It says: `If one of the selected bits is set, the channel is set to INVALID.' Sound good to me, and should work for Namur purposes I think? Does anyone have any experience with these advanced confiugration settings during the GSD file import?
our customer is going to use some IO-cards from Pepperl Fuchs for Namur porposes. These io-cards have a line fault detection for every input, see bit structure below.

One way to use this Line Fault is to create a second BoolIO for every input and give an error on the Line Fault when this occurs. But I also found another option when I click 'Advanced Configuration' in the Custimize input area. See printscreen below:

If I use this, I don't have to program a second boolIO for the Line Fault. But I never used the Advanced Settings before. It says: `If one of the selected bits is set, the channel is set to INVALID.' Sound good to me, and should work for Namur purposes I think? Does anyone have any experience with these advanced confiugration settings during the GSD file import?
Answers
This question has not yet been answered.
Add new comment