800xA 6.0 Mulitiple user simultaneous login impact on Workplace opening at Servers
For 800xA 6.0 system, can multiple users login and open Workplace simulataneously using Windows Remote Desktop on a single machine?
For example on AS1, if there is a user logged in as Operator from a remote desktop session, can there be a simultaneous login by an Engineer locally at the server?The operator is using OWPL and the engineer is using EWPL (using service account or engineer account login)
Where would be the best place to find the above information? Any help would be much appreciated. Many Thanks!
Answers
This is a windows question. 800xA doesn't care. It depends on the Operating System ....
Win 7 / Win 10 .... No, only 1 user
Win Server .... Usually 1, but you can increase this ... https://support.managed.com/kb/a1816/...
Windows Terminal Server .... Many, but practically about 4. It depends on how much memory and CPU you have available. (And TS Licenses)
There are many good reasons NOT to use the Aspect Servers and Connectivity servers for running operator workplaces. But basically, you are more likely to have to re-boot stations that people log on to regularly. If you want your servers to run for very long periods of time without being rebooted, don't use them as operator stations.
Win 7 / Win 10 .... No, only 1 user
Win Server .... Usually 1, but you can increase this ... https://support.managed.com/kb/a1816/...
Windows Terminal Server .... Many, but practically about 4. It depends on how much memory and CPU you have available. (And TS Licenses)
There are many good reasons NOT to use the Aspect Servers and Connectivity servers for running operator workplaces. But basically, you are more likely to have to re-boot stations that people log on to regularly. If you want your servers to run for very long periods of time without being rebooted, don't use them as operator stations.
Hello,
You can use same machine by different login (like rdp and local) simultaneously but ensure hardware specs should have more gig, hyper thread enabled and more than recommended RAM for better performance and gig network backbone
You can use same machine by different login (like rdp and local) simultaneously but ensure hardware specs should have more gig, hyper thread enabled and more than recommended RAM for better performance and gig network backbone
Add new comment