Unable to Deploy the EWS (Laptop Windows 10 pro) Error Code -1967456156 (0x8abb0064)
Dear Members
I want to connect Dell laptop as(Windows 10 pro ,Version 1709, Build 16299.64) EWS in to my Workgroup. Initial Settings , Prerequisites and ABB800xa 6.0.3 installation done without error. When deploying from ASCS1 the operation failed with error Code -1967456156 (0x8abb0064). log files enclosed.
How to overcome this issue?, your suggestions are most welcome.
Advance Thanks to All
Answers
i had simular problem with "-"in the netbios Name.
I think the "-"in the name is the problem.
Martin
I think the "-"in the name is the problem.
Martin
Hello,
The error code 0x8ABB0064 basically means that connection to the server has failed.

I would suggest you to:-
-> Check for correct NIC configurations on your EWS node.
-> Check RNRP.
-> Check for correct network adaptors' binding order.
-> Try to manually add the EWS node name and IP address in the Host file of ASCS1.
The error code 0x8ABB0064 basically means that connection to the server has failed.

I would suggest you to:-
-> Check for correct NIC configurations on your EWS node.
-> Check RNRP.
-> Check for correct network adaptors' binding order.
-> Try to manually add the EWS node name and IP address in the Host file of ASCS1.
I think you have to reset your Windows 10 to default and start again without the - in the name. The installer is looking for the old name now but can’t find that anymore.
Check your network sharing settings are enabled.
Also check that the following services - uPNP and SSDP services are running.
Also check that the following services - uPNP and SSDP services are running.
Add new comment