Set system 901F
Hello!
I have a PM901F CPU which I can't set the system time in (it's only one CPU in this network). The version of Freelance is 2016 SP1 with RU2. Operating system in the computers are Windows 10.
I have read earlier questions similar to this case.
Subnet mask is 255.255.240.0
When I try to set the system time it looks like below

I press "Ok" and every thing seems to work.
If i look at the CPU:s time variable it tell me that nothing have happen. The system time haven't changed at all.

Is there anyone who can tell me what to do? Maybe I have forgot something?
I have a PM901F CPU which I can't set the system time in (it's only one CPU in this network). The version of Freelance is 2016 SP1 with RU2. Operating system in the computers are Windows 10.
I have read earlier questions similar to this case.
Subnet mask is 255.255.240.0
When I try to set the system time it looks like below

I press "Ok" and every thing seems to work.
If i look at the CPU:s time variable it tell me that nothing have happen. The system time haven't changed at all.

Is there anyone who can tell me what to do? Maybe I have forgot something?
Answers
Try the following: On your engineering PC run the tool "Settings" from Freelance as Admin (right click, run as admin) and in the General Settings set the Enable Time synch. If it was already set, disable it and enable it again. Then press apply and ok. Restart the PC and try to set the controllers system time. See if it works this time
by Dieter Henkel
That is very strange. Is there maybe another Controller on the same network, which is just not configured in your current project? Or is the PS1 by chance connected to a radio clock?
by haab Rank: 1013 on 9/12/2018 6:50:57 AM | Like (0) | Report
There is no other Freelance Controller, but there is an AC500 controller (PM573-ETH) on the same network. This system is used as a safety system. These two system don´t communicate with each other on the Ethernet network. The only reason for the PM573-ETH to be on this network is so we reach it with it's programming tool. These two system communicate with each other with Profibus DP. The AC500-system is a Profibus slave under the Freelance Controller.
Add new comment