800xA Graphic Display resolution.
Dear Friends,
My VM backup of 800xA V5.1 resolution is 1366*768 but Actual Desktop which is in site resolution is 1920*1080.
Try to develop the screens in VM backup and import that to original system. How to solve the resolution issue?
Thanks in advance.
My VM backup of 800xA V5.1 resolution is 1366*768 but Actual Desktop which is in site resolution is 1920*1080.
Try to develop the screens in VM backup and import that to original system. How to solve the resolution issue?
Thanks in advance.
Answers
If you are developing new graphics, for site machine with display resolution 1920x1080, you can create the same in your VM machine. Set the graphics Width as 1920 and height as around 830 (remaining height 250 for Application Bar which shall include your Alarm Line, Date & Time, etc.). Later you can Export these graphics and Import to the site machine.
Hope this helps.
Hope this helps.
I guess that you are not able to set the graphic resolution in your VM to higher value and that's why you ask this question.
You have to enhance the memory of your "graphic card". In VMWare Workstation check the "Display" settings:

![]()
With ESXi server check the settings of the "Video card", you can use the Video Memory Calculator" for the proper settings. Keep in mind that you can change these settings only if you stop your VM.

/Erik
You have to enhance the memory of your "graphic card". In VMWare Workstation check the "Display" settings:
With ESXi server check the settings of the "Video card", you can use the Video Memory Calculator" for the proper settings. Keep in mind that you can change these settings only if you stop your VM.
/Erik
Your configuration may look different, but you have the (smaller) laptop screen and a (bigger) additional screen. Try to set the bigger one as main display. If this not help then disable the laptop display. (sorry, I have only the german version at hand)

![]()
Add new comment