Import and export .
Hi Mr. Rob,
I am working on project A - 800xA System 6.0.3.1(beginner level).
Can i create a project B screens,object structure, control structure in project A? Then export from A and import to B possible?
Kindly suggest a 800xA user manual related to import & export.
I am working on project A - 800xA System 6.0.3.1(beginner level).
Can i create a project B screens,object structure, control structure in project A? Then export from A and import to B possible?
Kindly suggest a 800xA user manual related to import & export.
Voted best answer
Yes you can export most objects/aspects from one system an import to another system. See Maintenance Manual for details of the tool. (3BSE046786-600)
In most cases you will export with "include children". Please be careful with "include dependencies", you will get large files with a lot of stuff from different structures. You should know what you do if you use this.
/Erik
In most cases you will export with "include children". Please be careful with "include dependencies", you will get large files with a lot of stuff from different structures. You should know what you do if you use this.
/Erik
Answers
Hello,
Yes you can do this using ABB Import Export tool. You can create your graphics, object types and logic in a different system and then using Import Export tool, copy the same into another system. But, you need to make sure that both these systems have the same Software installed and same System Extensions loaded.
You can launch Import Export tool from Plant Explorer Workplace or Engineering Workplace and then click on Help for more information on this tool. Please refer attached screenshots for you reference.
Hope this helps. :)
Yes you can do this using ABB Import Export tool. You can create your graphics, object types and logic in a different system and then using Import Export tool, copy the same into another system. But, you need to make sure that both these systems have the same Software installed and same System Extensions loaded.
You can launch Import Export tool from Plant Explorer Workplace or Engineering Workplace and then click on Help for more information on this tool. Please refer attached screenshots for you reference.
Hope this helps. :)
Add new comment