Sattline dual network cards in virtual machine
I have a virtual machine with win8.1 enterprise and sattline 2.5.6. The problem is that I want two networks and sattline use the wrong one!
Is there some way to configure sattline to choose the correct network?
I have tried in windows to change priority for the card, and also to untick automatic metric and set to fixed number but without success.

I want the marked IP address
Is there someone with some useful tips or ideas how to get this fixed?
Is there some way to configure sattline to choose the correct network?
I have tried in windows to change priority for the card, and also to untick automatic metric and set to fixed number but without success.

I want the marked IP address
Is there someone with some useful tips or ideas how to get this fixed?
Answers
The solution is to define an environment variable named SL_PrefSysId and set the value to the IP address that should be used by SattLine. During startup SattLine looks for the environment variable, and if found and the value has a valid IP address format and is found on one of the network interfaces on the machine, it will be used for system identity.
So defining environment variable SL_PrefSysId (Control Panel ->System->Advanced system settings -> Environment Variables), setting the value to 192.168.16.36 and restarting Sattline should solve your problem.
Add new comment