PG2 Graphic User access
Do we have any option, in 800xA PG2 graphics, when a user log-in as particular user (ex Operator user) , then set a variable to true in AC000M Controller?
The system version is SV6.0 .1 .
Since these information need to pass to third party system saying Operator used lodged-in ABB system.
The system version is SV6.0 .1 .
Since these information need to pass to third party system saying Operator used lodged-in ABB system.
Voted best answer
You can try an expression Variable as "User_Detect" and write an expression as if "x" user = " x user name" then Variable User_Detect as true.
Then try to use property transfer option to move this variable inside CBM.
Hope it should work.
Then try to use property transfer option to move this variable inside CBM.
Hope it should work.
Answers
i hope the attached screen shot/process will support your requirement
Please post for any clarification
Please post for any clarification
Add new comment