System Extension Maintenance for upgrade package 800xA System
I've upgrade the package of control system, as I refer to manual post installation, that we should deploy our package for new system. I check on System extension maintenance, it has 2 item that need to upgrade, first is AC800M Connect and AC800M High Integrity. System update from "5.1.0" to "5.1.1". But when I tried to update it says "This System Extension has a dependency to the Central Licensing System Extension V5.1.1 revision difference (error)".

As I follow manual I already release all the reservation on control builder and Plant explorer, but still can't update. Please advise or maybe any point I missed. I also attached Control Builder version, Soft Controller version and OPC Server version.

Voted best answer
According to the System Revisions document(s) I referred to in my answer above, Control Builder M Professional 5.1.0/1 (Build ID: 5.1.100.13) is part of System 800xA 5.1 RevB.
I assume you have access to proper media (a plastic box containing a set of roughly 10 DVD) or ISO-images of the same?
Inside the 5.1 FP4 RevE media box is a A4 sized paper with a notice covering possible upgrade paths and some instructions.
The upgrade can be made fully manually, or via an automated tool, the Feature Update Tool, FUT. With few software kits onboard, the upgrade is probably faster without using the FUT. With increasing number of options, the FUT becomes a more attractive option (of course, also depending on your skill set). Also, the FUT is automated.
For specfic instructions regarding the FUT, download the most recent System 800xA 5.1 System Feature Pack Update Tool, 2PAA107435-511, Rev H.
For general upgrade instructions, download the most recent System 800xA 5.1 Upgrade User's Guide, 3BSE036342-511, RevG.
Answers
Perhaps you can show us a picture of System Extension from Admin Structure and also from Configuration Wizards Load Extension?
Based on your CBM 5.1.1-4 (Build 5.1.1400.15), I guess that you are running SV5.1 FP4 RevE.
Reference: 3BSE056732 "System 800xA 5.1 System Software Versions"
According to 3BSE056732 for SV5.1 FP4 RevE the following applies:
ABB Central Licensing System Extension 5.1.0-6 Build Id 5.1.5624.16310
Please check that this version of "Central Licensing System Extension" is installed and loaded.
BR Carsten
Thanks for the answer, first I create virtual machine from running system, so system not connected to PC which hold the license.
Here I attach picture :

For snapshot Admin Structure :

Is it because not connected to license server, so it can't be upgraded to ver 5.1.1? please advise. Thanks for the support.
What revision are you on?
5.1 no revision/featurepack
5.1 Rev A, B, C, D or E
5.1 FP1, FP2, FP3, FP4RevC, FP4RevD or FP4RevE
Really, there is no option to "pick & choose" individual software kits from the System 800xA suite here - you must stick to versions belonging to a known revision - see the System 800xA 5.1 System Revisions, 3BSE056732 document on ABB Library for a list of supported "combinations".
Hi Stefan,
I check manual for upgrade installation, I missed out to deploy full package installation first before install "Control Package Upgrade" . So My System
base software is "5.1.0/1 ( 5.1.100.13)".
My question, can I upgrade directly to "5.1 Rev" E and then continue to install 5.1 FP4REV E ? .
Or I can directly install to 5.1 FP4REVE ?, because I tried to install 5.1FP4REVE, it prompt out ERROR, can't find location path for 5.1FP3.
Or I should install step by step from closes system to "5.1.0/1" ?
Regards,
DZ
Add new comment