OPC A800xA Synchronous or Asynchronous.
Hi. Which mode OPC of A800Xa are using, Synchronous or Asynchronous ?
Thanks.
Thanks.
Answers
Please have a look at
3BDS011222 ,System 800xA Vx.x Configuration.
Under "Accessing 800xA via OPC " and "Integrating OPC Servers into 800xA" you find the supported versions of OPC and the restrictions.
/Erik
AFAIK:
On the input side (via the OPC DA Connector service when 800xA is the client): asynchronous
On the output side (via the ABB.OPCDAServer.1 or ABB.OPCDAServerSurrogate.1 when 800xA is the server): asynchronous or synchronous.
Add new comment