How to load a program to ABB500 -eco PLC.
Hello, I have written a program which runs fine in the simulation and I want to load this program tp the PLC CPU. Could anyone guide me with the steps that I need to follow?
Answers
Greetings,
There are some video tutorials exist on youtube:
https://youtu.be/L0HhKEg7vEI
https://youtu.be/sIUFx0tG0Hk
Hope these help you.
There are some video tutorials exist on youtube:
https://youtu.be/L0HhKEg7vEI
https://youtu.be/sIUFx0tG0Hk
Hope these help you.
Hi
in addition to the good suggestion of Titus, to give you a correct sequence to download the program in to the cpu, you need to specify your type of cpu - Eth or not Eth - and the version of the Automation Builder that you are using.
Depending on the type of the PLC you have different setting of cpu to define in AB - such IP adress if you are using Eth version - or communication setting if you are using USB-COM port.
If you give us more information, we can help you better
in addition to the good suggestion of Titus, to give you a correct sequence to download the program in to the cpu, you need to specify your type of cpu - Eth or not Eth - and the version of the Automation Builder that you are using.
Depending on the type of the PLC you have different setting of cpu to define in AB - such IP adress if you are using Eth version - or communication setting if you are using USB-COM port.
If you give us more information, we can help you better
Add new comment