Starting workplace with non-admin user
Voted best answer
Hi, I had the same problem with Windows 10 (WORKGROUP). I added new user and this message (Impersonate a client after authentication privilege missing. Log over is not possible) came up during opening workplace.
You have to follow these procedure:
1. Go to Start > Control Panel > Administrative Tools and then select Local Security Policy.
2. Expand Local Policy, and click User Rights Assignment.
3. In the right panel, double-click Impersonate a client after authentication.
4. In the Local Security Policy Setting dialog box, click Add. Use Windows File security to protect the applications above from being launched by unauthorized users. Digital Signature Section 4 Security Configurations 126 3BSE037410-510 D
5. In the Select Users or Group dialog box, click the user account the you want to add, click Add and then OK.
You have to follow these procedure:
1. Go to Start > Control Panel > Administrative Tools and then select Local Security Policy.
2. Expand Local Policy, and click User Rights Assignment.
3. In the right panel, double-click Impersonate a client after authentication.
4. In the Local Security Policy Setting dialog box, click Add. Use Windows File security to protect the applications above from being launched by unauthorized users. Digital Signature Section 4 Security Configurations 126 3BSE037410-510 D
5. In the Select Users or Group dialog box, click the user account the you want to add, click Add and then OK.
Answers
This comes when Pre-requisites are not done correctly.
Try the following from Your Primary Domain Server
Goto Control Panel -> User Accounts -> User Accounts Control Settings
Select "Never Notify"
Try the following from Your Primary Domain Server
Goto Control Panel -> User Accounts -> User Accounts Control Settings
Select "Never Notify"
Hi,
this behavior is quite common, UAC must be disabled on the computer where you want to run Workplace. Changing UAC to "do not notify" usually does not help.
It must be disabled in registry and computer must be rebooted.
![]()
this behavior is quite common, UAC must be disabled on the computer where you want to run Workplace. Changing UAC to "do not notify" usually does not help.
It must be disabled in registry and computer must be rebooted.
So, just open regedit and locate this key.
HKEY LOCAL MACHINE\SOFTWARE\Microsoft\Windows\currentversion\Policies\system
In the right pane look for EnableLUA and modify its value to 0. Close regedit.
Done.
Do the UAC policies in domain controller.
Hi,
System 800xA supports Windows UAC (User Account Control) in default state. Installation and configuration needs administrator privileges whereas normal operation should be performed with standard user privileges to maintain a secure operation environment.
You can disable User Account Control "Never Notify" through control panel.
Also disable it from registry as said by Antonin.
Let us know your observations
Hope that helps
System 800xA supports Windows UAC (User Account Control) in default state. Installation and configuration needs administrator privileges whereas normal operation should be performed with standard user privileges to maintain a secure operation environment.
You can disable User Account Control "Never Notify" through control panel.
Also disable it from registry as said by Antonin.
Let us know your observations
Hope that helps
I'm assuming CHMI is Compact HMI and that you are running in a Workgroup with only local local security. The actions you are seeing, if everything was loaded correctly and setup as per manuals, is that the user logging in and trying to open a Workplace does not have their security policies sync'd with 800xA (CHMI). That is you have a user setup in Windows but this has not been replicated into the CHMI (800xA Users) setup. Please check the manuals on correct way to setup users especially when setting Operations vs Admins.
From this Non-Admin user account, access the path: HKEY LOCAL MACHINE\SOFTWARE\Microsoft\Windows\currentversion\Policies\system from registry editor (regedit) and check if registry: EnableLUA is set to 1. If so, change it to 0 and reboot the node.
Do share the result.
Do share the result.
Impersonate a client after authentication , add IndustrialITuser to Administrative templates->Local security policy->USer rights assignment->industrial IT user should be added and restart workplace
by AbdelrazzaqHiasat Rank: 172 on 7/31/2018 10:34:33 PM | Like (0) | Report
Thank you all for your support.
After disabling User Account Control , and editing the registry, I could start the workplace. but every time i start it i get the following information message : " impersonate a client after authentication privilege missing log over is not possible "
by aravind12a6 Rank: 152 on 8/1/2018 9:41:31 PM | Like (1) | Report
Impersonate a client after authentication , add IndustrialITuser to Administrative templates->Local security policy->USer rights assignment->industrial IT user should be added and restart workplace
by AbdelrazzaqHiasat Rank: 172 on 8/7/2018 11:46:26 PM | Like (0) | Report
"add IndustrialITuser to Administrative templates" how can i do that? Do i need .admx file?
can you please clarify?
by AbdelrazzaqHiasat Rank: 172 on 8/7/2018 11:55:48 PM | Like (0) | Report
@aravind12a6 I solved the issure, thank you.
Add new comment