800xA 6032 Deploy successful, But clients and some are not connected to system
HI I am setting up a new 800xA6032 system from 6031 system backup. I followed the procedure Move a system from 2PAA111708-600 N. The deploy went well for all the servers and clients without any errors.
But some of the clients and servers are not connected to the system. All these servers and clients shows 'Needs Redeploy' in System configuration Console. If i try to redeploy the deploy window is empty. So it is not possible to redeploy.
Note: Some other servers are deployed correctly and shows deployed in SCC and they have the system as well.
But some of the clients and servers are not connected to the system. All these servers and clients shows 'Needs Redeploy' in System configuration Console. If i try to redeploy the deploy window is empty. So it is not possible to redeploy.
Note: Some other servers are deployed correctly and shows deployed in SCC and they have the system as well.
Answers
This question has not yet been answered.
Add new comment