Please read - ABB Central Licensing System 6.0.3-0 RU2 released on JUL 11th contains an error
See this thread:
https://forum-controlsystems.abb.com/...
The corruption is likely only giving a small marginal warning (Inconsistent Media) in the Configure System task of SCC (no operational proplems noticed, so far)
https://forum-controlsystems.abb.com/...
The corruption is likely only giving a small marginal warning (Inconsistent Media) in the Configure System task of SCC (no operational proplems noticed, so far)
Answers
There is a simple editorial error in a core package file (C:\ProgramData\ABB\800xA\MediaRepository\Core\Licensing\ABB_CLS_Installer_Proje
ct.corepackage) which needs to be corrected.
I assume the corrupt rollup will be revoked and a new corrected one be published on ABB Library shortly.
Once the new rollup is out, affected systems can easily be repaired by copying the above file from the corrected media over to the LRU on each machine.
Systems affected should not see any other issue from this problem with exception for the warning in Configure System.
ct.corepackage) which needs to be corrected.
I assume the corrupt rollup will be revoked and a new corrected one be published on ABB Library shortly.
Once the new rollup is out, affected systems can easily be repaired by copying the above file from the corrected media over to the LRU on each machine.
Systems affected should not see any other issue from this problem with exception for the warning in Configure System.
Add new comment