VB empty graphics clean up in 6.0.3.2
Hello,
We have upgrade the system from xA5.0 sp2 to xA6.0.3.2 in the following method without errors:
1.Upgraded the system from xA5.0 sp2 to xA5.1 Rev E and migrated the graphics from VB to PG2.
2.Upgraded the system from xA5.1 rev E to xA6.0.3.2
Now in xA6.0.3.2 we finding empty VB graphics "no longer support" so shall we delete these graphics?
If so is there any tool to remove all VB graphics.
tried using VBremoval tool it removes only extensions not the graphics.
We have upgrade the system from xA5.0 sp2 to xA6.0.3.2 in the following method without errors:
1.Upgraded the system from xA5.0 sp2 to xA5.1 Rev E and migrated the graphics from VB to PG2.
2.Upgraded the system from xA5.1 rev E to xA6.0.3.2
Now in xA6.0.3.2 we finding empty VB graphics "no longer support" so shall we delete these graphics?
If so is there any tool to remove all VB graphics.
tried using VBremoval tool it removes only extensions not the graphics.
Answers
Import of VB6 is no longer possible; aspects become "nullified" but not removed.
Will check and revert what the long term plan is for these "tombstones"...
... vacation period here... few to ask...
Hi
Yes, you can delete the VB Graphics and Elements after making sure that None PG2 Graphics & Elements have no references to any of the VB aspects. Refer System 800xA VBPG migration and System 800xA VBPG Search Tool (3BSE081093).
Best Regards
Yes, you can delete the VB Graphics and Elements after making sure that None PG2 Graphics & Elements have no references to any of the VB aspects. Refer System 800xA VBPG migration and System 800xA VBPG Search Tool (3BSE081093).
Best Regards
I have put all the vb items in a temporary extension library for items in libraries. And then deleted the extension library. Then I used a combination of bulk data manager and the search tool with shift (pressed) while selecting a start and an end item then delete. ctrl + a works only correct with a small list in the search tool.
That will get rid of the vb stuff quickly.
That will get rid of the vb stuff quickly.
Add new comment