Ac500 export symbol file mene
We install automation builder, last version but in the menue applicaction export to generate symbol file does not appears,
it is any way to enable this menu?
it is any way to enable this menu?
Voted best answer
I'd say something went wrong during installation and would suggest to un-install and then re-install Automation Builder.
I've tried to create a project from scratch and even if you have only hardware configuration in project the menu item is still there, though if you try to click it - it'll give you an error saying no symbol file was configured.
I've tried to create a project from scratch and even if you have only hardware configuration in project the menu item is still there, though if you try to click it - it'll give you an error saying no symbol file was configured.
Answers
Hi
I'm not be sure if your question is about to use the symbol file - generation tag - with one CP600 or CP600 eCo panel
If yes, you can find the complete instruction to generate it from Codesys in the CP600 panel - 3ADR059001M0210 document, available in library.
Hope this help you
I'm not be sure if your question is about to use the symbol file - generation tag - with one CP600 or CP600 eCo panel
If yes, you can find the complete instruction to generate it from Codesys in the CP600 panel - 3ADR059001M0210 document, available in library.
Hope this help you
Add new comment