Import/Export Object Failure
using:
OperateIT build 102a
Import/Export Wizard ver 0.1.2.0
If you create an object under the object structure, and export the entire object to an afw file, Delete the Object from the oBject structure, then try to import the entire object, the import will fail with "internal Error 0x80090057"
If you manually recreate the object you can successfully import just the aspects for the object.
OperateIT build 102a
Import/Export Wizard ver 0.1.2.0
If you create an object under the object structure, and export the entire object to an afw file, Delete the Object from the oBject structure, then try to import the entire object, the import will fail with "internal Error 0x80090057"
If you manually recreate the object you can successfully import just the aspects for the object.
Answers
On w103a_2 I've done the following:
1) Created an Object Type "test" with one General Properties Aspect
2) Exported "test"
3) Deleted "test"
4) Imported "test"
Everything worked fine
a) either the problem has be fixed in w103a_2
b) or we need more context
I will forward the problem to an import/export expert
1) Created an Object Type "test" with one General Properties Aspect
2) Exported "test"
3) Deleted "test"
4) Imported "test"
Everything worked fine
a) either the problem has be fixed in w103a_2
b) or we need more context
I will forward the problem to an import/export expert
Add new comment